Data structure of the receivers_list event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::elem_index
Client model element index
Definition at line
18329
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::server_address
Unicast address of the server
Definition at line
18330
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::index
Index of the entry reported
Definition at line
18331
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
nodes_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::nodes_list_size
Number of entries currently in the node list
Definition at line
18332
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
address#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::address
Address of the Update Server
Definition at line
18333
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
phase#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::phase
Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Phase of the Update Server
Definition at line
18334
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_status#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::update_status
Last Update Status message received from the Update Server
Definition at line
18337
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_status#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::transfer_status
Last Transfer Status message received from the BLOB Transfer Server
Definition at line
18339
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
progress#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::progress
0-100, percentage of BLOB Transfer octets delivered and confirmed
Definition at line
18341
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::fw_index
Index of the firmware being updated
Definition at line
18343
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h