Data structure of the upload_complete event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_upload_complete_s::elem_index

Client model element index


Definition at line 18535 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_upload_complete_s::server_address

Unicast address of the server


Definition at line 18536 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_client_upload_complete_s::blob_id

The ID of the BLOB.


Definition at line 18537 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_size#

uint32_t sl_btmesh_evt_fw_dist_client_upload_complete_s::blob_size

The size of the BLOB.


Definition at line 18538 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fwid#

uint8array sl_btmesh_evt_fw_dist_client_upload_complete_s::fwid

FWID of the firmware that was uploaded.


Definition at line 18539 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h