Data structure of the dist_start_req event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::elem_index

Server model element index


Definition at line 17327 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::client_address

Address of the Distribution Client


Definition at line 17328 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

group_address#

uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::group_address

Group address of the distribution


Definition at line 17329 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

virtual_address#

uuid_128 sl_btmesh_evt_fw_dist_server_dist_start_req_s::virtual_address

If the group address is a VA hash, this contains the full virtual address label UUID of the distribution. Otherwise, the value of this field should be ignored.


Definition at line 17330 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ttl#

uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::ttl

Distribution TTL


Definition at line 17334 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

apply_immediately#

uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::apply_immediately

Enum sl_btmesh_fw_dist_server_dfu_policy_t. 1 if the Update Policy is Verify and Apply, otherwise 0.


Definition at line 17335 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fw_list_index#

uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::fw_list_index

Index of the firmware in the Distributor's FW List


Definition at line 17339 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timeout_base#

uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::timeout_base

Timeout base


Definition at line 17341 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_mode#

uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::transfer_mode

Transfer Mode to use in the distribution


Definition at line 17342 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h