Data structure of the dist_state_changed event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_dist_state_changed_s::elem_index
Server model element index
Definition at line
17477
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
state#
uint8_t sl_btmesh_evt_fw_dist_server_dist_state_changed_s::state
Enum sl_btmesh_fw_dist_server_dist_step_t. New state of the Distribution
Definition at line
17478
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
num_active_nodes#
uint16_t sl_btmesh_evt_fw_dist_server_dist_state_changed_s::num_active_nodes
Number of active nodes
Definition at line
17481
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h