Data structure of the upload_complete event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_upload_complete_s::elem_index

Server model element index


client_address#

uint16_t sl_btmesh_evt_fw_dist_server_upload_complete_s::client_address

Address of the Distribution Client


size#

uint32_t sl_btmesh_evt_fw_dist_server_upload_complete_s::size

Upload size


blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_server_upload_complete_s::blob_id

BLOB ID


fwid#

uint8array sl_btmesh_evt_fw_dist_server_upload_complete_s::fwid

FWID of the firmware image