Data structure of the upload_start_metadata event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::elem_index
Server model element index
Definition at line
17407
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::client_address
Address of the Distribution Client
Definition at line
17408
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
metadata#
uint8array sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::metadata
Metadata of the FW
Definition at line
17409
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h