Data structure of the dist_state_changed event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_standalone_updater_dist_state_changed_s::elem_index

Element index


Definition at line 19787 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

state#

uint8_t sl_btmesh_evt_fw_standalone_updater_dist_state_changed_s::state

Enum sl_btmesh_fw_dist_server_dist_step_t. New state of the Distribution


Definition at line 19788 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

num_active_nodes#

uint16_t sl_btmesh_evt_fw_standalone_updater_dist_state_changed_s::num_active_nodes

Number of active nodes


Definition at line 19791 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h