Data structure of the check_fw_metadata_req event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::elem_index

Server model element index


client_address#

uint16_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::client_address

Address of the Update Client


fw_index#

uint8_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::fw_index

Index of the currently installed firmware to check for updating.


metadata#

uint8array sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::metadata

Metadata for the incoming firmware. May be zero-length.