Data structure of the update_start_req event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::elem_index

Server model element index


client_address#

uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::client_address

Address of the Update Client


blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_fw_update_server_update_start_req_s::blob_id

BLOB ID of the firmware being transferred.


fw_index#

uint8_t sl_btmesh_evt_fw_update_server_update_start_req_s::fw_index

Index of the firmware to update


metadata#

uint8array sl_btmesh_evt_fw_update_server_update_start_req_s::metadata

Metadata for the FWID in the following update_start_req event. May be zero-length.