Data structure of the om_status event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_client_om_status_s::destination_address

Address of the client or the group address to which it was published.


elem_index#

uint16_t sl_btmesh_evt_lc_client_om_status_s::elem_index

Index of the element for which received the status.


server_address#

uint16_t sl_btmesh_evt_lc_client_om_status_s::server_address

Device which sent the status.


appkey_index#

uint16_t sl_btmesh_evt_lc_client_om_status_s::appkey_index

Appkey used by server_address.


om_status_value#

uint8_t sl_btmesh_evt_lc_client_om_status_s::om_status_value

Value reported by server.