Data structure of the property_status event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_client_property_status_s::destination_address
Address of the client or the group address to which it was published.
elem_index#
uint16_t sl_btmesh_evt_lc_client_property_status_s::elem_index
Index of the element for which received the status.
server_address#
uint16_t sl_btmesh_evt_lc_client_property_status_s::server_address
Device which sent the status.
appkey_index#
uint16_t sl_btmesh_evt_lc_client_property_status_s::appkey_index
Appkey used by server_address.