Data structure of the ambient_lux_level_updated event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::destination_address
Message destination address
elem_index#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::elem_index
Index of the element where the update happened
source_address#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::source_address
Message source address
appkey_index#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::appkey_index
Message appkey index
ambient_lux_level_value#
uint32_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::ambient_lux_level_value
The updated value of the LC Ambient LuxLevel state