Data structure of the occupancy_updated event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::destination_address
Message destination address if triggered by a message, 0 otherwise.
elem_index#
uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::elem_index
Index of the element where the update happened
source_address#
uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::source_address
Message source address if triggered by a message, 0 otherwise.
appkey_index#
uint16_t sl_btmesh_evt_lc_server_occupancy_updated_s::appkey_index
Message appkey index if triggered by a message, 0xFFFF otherwise.
occupancy_value#
uint8_t sl_btmesh_evt_lc_server_occupancy_updated_s::occupancy_value
The updated value of the LC Occupancy state