Data structure of the regulator_debug_info event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_lc_server_regulator_debug_info_s::elem_index

Index of the element where LC server is located


Definition at line 14171 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

i#

uint16_t sl_btmesh_evt_lc_server_regulator_debug_info_s::i

Integral term


Definition at line 14172 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

l#

uint16_t sl_btmesh_evt_lc_server_regulator_debug_info_s::l

Regulator output


Definition at line 14173 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h