sl_btmesh_evt_lpn_friendship_failed#

Indicate that the friendship establishment has failed, received as a response to the sl_btmesh_lpn_establish_friendship command.

Modules#

sl_btmesh_evt_lpn_friendship_failed_s

Macros#

#define

Identifier of the friendship_failed event.

Typedef Documentation#

sl_btmesh_evt_lpn_friendship_failed_t#

typedef struct sl_btmesh_evt_lpn_friendship_failed_s sl_btmesh_evt_lpn_friendship_failed_t

Definition at line 7665 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_lpn_friendship_failed_id#

#define sl_btmesh_evt_lpn_friendship_failed_id
Value:
0x012300a8

Identifier of the friendship_failed event.


Definition at line 7654 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h