Data structure of the send_chunk_request event.

Public Attributes#

uint16_t
uint32_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_client_send_chunk_request_s::elem_index

The client model element index.


Definition at line 10451 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

offset#

uint32_t sl_btmesh_evt_mbt_client_send_chunk_request_s::offset

The chunk offset from the beginning of the BLOB.


Definition at line 10452 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

length#

uint16_t sl_btmesh_evt_mbt_client_send_chunk_request_s::length

The number of bytes requested.


Definition at line 10453 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h