You are viewing documentation for version:
Data structure of the server_failed event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_server_failed_s::elem_index
The client model element index.
server_address#
uint16_t sl_btmesh_evt_mbt_client_server_failed_s::server_address
The MBT Server address.
timeout#
uint8_t sl_btmesh_evt_mbt_client_server_failed_s::timeout
Non-zero if a timeout occurred.
error#
uint8_t sl_btmesh_evt_mbt_client_server_failed_s::error
Non-zero if an error occurred.