Data structure of the start_block_complete event.

Public Attributes#

uint16_t
uint16_t
uint32_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_client_start_block_complete_s::elem_index

The client model element index.


Definition at line 10424 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_number#

uint16_t sl_btmesh_evt_mbt_client_start_block_complete_s::block_number

The index number of the block.


Definition at line 10425 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_size#

uint32_t sl_btmesh_evt_mbt_client_start_block_complete_s::block_size

The size of the block.


Definition at line 10426 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h