Data structure of the fw_added event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_ncp_fw_list_fw_added_s::elem_index

Server model element index


Definition at line 20252 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

size#

uint32_t sl_btmesh_evt_ncp_fw_list_fw_added_s::size

Size of the image


Definition at line 20253 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_ncp_fw_list_fw_added_s::blob_id

BLOB ID that will be used to transmit the image


Definition at line 20254 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fwid#

uint8array sl_btmesh_evt_ncp_fw_list_fw_added_s::fwid

Firmware ID of the image


Definition at line 20256 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h