Data structure of the private_gatt_proxy_status event.

Public Attributes#

uint16_t
uint32_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 21870 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::handle

Request handle


Definition at line 21871 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

value#

uint8_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::value

On-Demand Private GATT proxy value of the node. Valid values are:

  • 0: Advertising with Private Network Identity type cannot be enabled on demand

  • 1-255: Advertising interval for Private Network Identity in seconds


Definition at line 21872 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h