Data structure of the filter_status event.
Public Attribute Documentation#
handle#
uint32_t sl_btmesh_evt_proxy_filter_status_s::handle
Proxy handle
Definition at line
3591
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
type#
uint8_t sl_btmesh_evt_proxy_filter_status_s::type
Filter type: 0x00 to allow traffic from the given address, 0x01 to block traffic from the given address
Definition at line
3592
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
count#
uint16_t sl_btmesh_evt_proxy_filter_status_s::count
Current filter list length
Definition at line
3594
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h