Data structure of the link_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_remote_provisioning_client_link_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


server#

uint16_t sl_btmesh_evt_remote_provisioning_client_link_status_s::server

Server address.


status#

uint8_t sl_btmesh_evt_remote_provisioning_client_link_status_s::status

Enum sl_btmesh_remote_provisioning_server_status_t. server status.


state#

uint8_t sl_btmesh_evt_remote_provisioning_client_link_status_s::state

Enum sl_btmesh_remote_provisioning_client_link_state_t. link state.