Data structure of the scan_capabilities event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19165 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::server

Server address.


Definition at line 19166 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_items#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::max_items

The maximum number of UUIDs that can be reported during scanning.


Definition at line 19167 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

active#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::active

Indication if active scan is supported.


Definition at line 19169 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h