Data structure of the status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_client_status_s::destination_address

Address of the client or the group address to which it was published.


Definition at line 14474 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scene_client_status_s::elem_index

Index of the element which received the status.


Definition at line 14476 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_scene_client_status_s::server_address

Device which sent the status.


Definition at line 14478 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scene_client_status_s::appkey_index

Appkey used by client_address.


Definition at line 14479 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_scene_client_status_s::status

Status of the request.


Definition at line 14480 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

current_scene#

uint16_t sl_btmesh_evt_scene_client_status_s::current_scene

Currently selected scene.


Definition at line 14481 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

target_scene#

uint16_t sl_btmesh_evt_scene_client_status_s::target_scene

Scene to be transitioning to.


Definition at line 14482 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

remaining_time_ms#

uint32_t sl_btmesh_evt_scene_client_status_s::remaining_time_ms

Time (in milliseconds) remaining in transition.


Definition at line 14483 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h