Data structure of the compact_recall event.

Public Attributes#

Public Attribute Documentation#

states#

uint8array sl_btmesh_evt_scene_server_compact_recall_s::states

Byte array containind recalled states. Array consist of 5 byte chunks as follows:

  • Element id as 16bit unsigned integer in little endian format

  • Model id as 16bit unsigned integer in little endian format

  • Model-specific state type, identifying the kind of state recalled See get state types list for details.

after this event application can request recalled states with sl_btmesh_generic_server_get_cached_state command


Definition at line 14806 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h