Data structure of the get event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_server_get_s::destination_address

Address of the server or the group address to which it was published.


Definition at line 14700 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scene_server_get_s::elem_index

Index of the element which received the command.


Definition at line 14702 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_scene_server_get_s::client_address

Device which sent the request.


Definition at line 14704 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scene_server_get_s::appkey_index

Appkey used by client_address.


Definition at line 14705 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h