Data structure of the recall event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_scene_server_recall_s::destination_address
Address of the server or the group address to which it was published.
Definition at line
14752
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_scene_server_recall_s::elem_index
Index of the element which received the command.
Definition at line
14754
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
selected_scene#
uint16_t sl_btmesh_evt_scene_server_recall_s::selected_scene
Scene of interest
Definition at line
14756
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_scene_server_recall_s::client_address
Device which sent the request.
Definition at line
14757
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_scene_server_recall_s::appkey_index
Appkey used by client_address.
Definition at line
14758
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transition_time_ms#
uint32_t sl_btmesh_evt_scene_server_recall_s::transition_time_ms
Time (in milliseconds) allotted for the transition to take place
Definition at line
14759
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h