sl_btmesh_evt_scheduler_client_action_status#

Scheduler Action Status event, received as a response to the sl_btmesh_scheduler_client_set_action or sl_btmesh_scheduler_client_get_action command.

For the description of these fields, see Scheduler Server

Modules#

sl_btmesh_evt_scheduler_client_action_status_s

Macros#

#define

Identifier of the action_status event.

Typedef Documentation#

sl_btmesh_evt_scheduler_client_action_status_t#

typedef struct sl_btmesh_evt_scheduler_client_action_status_s sl_btmesh_evt_scheduler_client_action_status_t

Definition at line 15078 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_scheduler_client_action_status_id#

#define sl_btmesh_evt_scheduler_client_action_status_id
Value:
0x015400a8

Identifier of the action_status event.


Definition at line 15054 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h