Data structure of the action_changed event.
Public Attributes#
uint16_t
uint8_t
uint8_t
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint32_t
uint16_t
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_scheduler_server_action_changed_s::elem_index
Scheduler server model element index
Definition at line
15352
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::index
Index of the Scheduler Register
Definition at line
15353
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
year#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::year
Scheduled year for the action
Definition at line
15354
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
month#
uint16_t sl_btmesh_evt_scheduler_server_action_changed_s::month
Scheduled month for the action
Definition at line
15355
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
day#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::day
Scheduled day of the month for the action
Definition at line
15356
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
hour#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::hour
Scheduled hour for the action
Definition at line
15357
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
minute#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::minute
Scheduled minute for the action
Definition at line
15358
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
second#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::second
Scheduled second for the action
Definition at line
15359
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
day_of_week#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::day_of_week
Scheduled days of the week for the action
Definition at line
15360
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
action#
uint8_t sl_btmesh_evt_scheduler_server_action_changed_s::action
Action to be performed at the scheduled time
Definition at line
15361
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transition_time_ms#
uint32_t sl_btmesh_evt_scheduler_server_action_changed_s::transition_time_ms
Transition time for this action
Definition at line
15362
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
scene_number#
uint16_t sl_btmesh_evt_scheduler_server_action_changed_s::scene_number
Scene number to be used for some actions
Definition at line
15363
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h