Data structure of the action_triggered event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_scheduler_server_action_triggered_s::elem_index
Scheduler server model element index
Definition at line
15407
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint8_t sl_btmesh_evt_scheduler_server_action_triggered_s::index
Index of the Scheduler Register
Definition at line
15408
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
action#
uint8_t sl_btmesh_evt_scheduler_server_action_triggered_s::action
Action to be performed at the scheduled time
Definition at line
15409
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transition_time_ms#
uint32_t sl_btmesh_evt_scheduler_server_action_triggered_s::transition_time_ms
Transition time for this action
Definition at line
15410
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
scene_number#
uint16_t sl_btmesh_evt_scheduler_server_action_triggered_s::scene_number
Scene number to be used for some actions
Definition at line
15411
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h