Data structure of the scene_changed event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_scheduler_server_scene_changed_s::elem_index

Scheduler server model element index


Definition at line 15384 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transition_time_ms#

uint32_t sl_btmesh_evt_scheduler_server_scene_changed_s::transition_time_ms

Transition time for this action


Definition at line 15385 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scene_number#

uint16_t sl_btmesh_evt_scheduler_server_scene_changed_s::scene_number

Scene number being activated


Definition at line 15386 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h