Data structure of the publish event.

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_sensor_server_publish_s::elem_index

Client model element index


Definition at line 11749 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

period_ms#

uint32_t sl_btmesh_evt_sensor_server_publish_s::period_ms

The current publishing period that can be used to estimate the next tick, e.g., when the state should be reported at higher frequency.


Definition at line 11750 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h