Data structure of the get_settings_request event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

server_address#

uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::server_address

Address the request was directed to, either the server's unicast address or a group address the server subscribes to


Definition at line 12088 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::elem_index

Setup Server model element index


Definition at line 12091 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::client_address

Requesting client model's address


Definition at line 12092 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::appkey_index

The application key index to use


Definition at line 12093 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::flags

No flags defined currently


Definition at line 12094 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_setup_server_get_settings_request_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 12095 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h