sl_btmesh_evt_silabs_config_client_model_status#

TX over AE on per-model basis enable/disable state.

Received as a response to the sl_btmesh_silabs_config_client_set_model_enable and sl_btmesh_silabs_config_client_get_model_enable command.

Modules#

sl_btmesh_evt_silabs_config_client_model_status_s

Macros#

#define

Identifier of the model_status event.

Typedef Documentation#

sl_btmesh_evt_silabs_config_client_model_status_t#

typedef struct sl_btmesh_evt_silabs_config_client_model_status_s sl_btmesh_evt_silabs_config_client_model_status_t

Definition at line 3856 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_silabs_config_client_model_status_id#

#define sl_btmesh_evt_silabs_config_client_model_status_id
Value:
0x020100a8

Identifier of the model_status event.


Definition at line 3839 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h