Data structure of the items_status event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

src#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::src

Server address


Definition at line 21991 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

dst#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::dst

Client address


Definition at line 21992 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::appkey_index

App key index


Definition at line 21993 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

range_start#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_start

15 least significant bits of the starting unicast address


Definition at line 21994 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

length_present#

uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::length_present

Indicates the presence or absence of the RangeLength field


Definition at line 21996 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

range_length#

uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_length

If present, containsNumber of addresses in the range (0x02 – 0xFF), otherwise 0


Definition at line 21998 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h