Data structure of the replay_protection_list_entry_cleared event.

Public Attributes#

uint16_t

Public Attribute Documentation#

address#

uint16_t sl_btmesh_evt_test_replay_protection_list_entry_cleared_s::address

Source address for the replay protection list entry


Definition at line 6335 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h