Data structure of the replay_protection_list_saved event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6356 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

saved_count#

uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::saved_count

Number of entries saved successfully


Definition at line 6357 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

total_count#

uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::total_count

Number of entries in the list in total


Definition at line 6358 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h