Data structure of the tai_utc_delta_updated event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::elem_index

Server model element index


Definition at line 16218 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_utc_delta_current#

int32_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_utc_delta_current

Current difference between TAI and UTC is seconds. Range is -255 to 32512.


Definition at line 16219 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_utc_delta_new#

int32_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_utc_delta_new

Upcoming difference between TAI and UTC is seconds. Range is -255 to 32512.


Definition at line 16221 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_of_delta_change#

uint64_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_of_delta_change

TAI Seconds time of the upcoming TAI-UTC Delta change


Definition at line 16223 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h