Data structure of the time_role_updated event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_time_server_time_role_updated_s::elem_index

Server model element index


Definition at line 16246 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_role#

uint8_t sl_btmesh_evt_time_server_time_role_updated_s::time_role

Time Role


Definition at line 16247 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h