Data structure of the send_complete event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_vendor_model_send_complete_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 4178 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint16_t sl_btmesh_evt_vendor_model_send_complete_s::handle

Tracking handle for the message sending attempt as reported by sl_btmesh_vendor_model_send_tracked or sl_btmesh_vendor_model_set_publication_tracked command responses.


Definition at line 4179 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

message_flags#

uint8_t sl_btmesh_evt_vendor_model_send_complete_s::message_flags

Unsigned 8-bit integer


Definition at line 4184 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h