Data structure of the friend_relay event.
Public Attribute Documentation#
netkey_index#
uint16_t sl_btmesh_evt_diagnostic_friend_relay_s::netkey_index
Index of the network key used in friendship
Definition at line
22495
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
lpn#
uint16_t sl_btmesh_evt_diagnostic_friend_relay_s::lpn
LPN address
Definition at line
22496
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
src#
uint16_t sl_btmesh_evt_diagnostic_friend_relay_s::src
Source address of the message
Definition at line
22497
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
dst#
uint16_t sl_btmesh_evt_diagnostic_friend_relay_s::dst
Destination address of the message
Definition at line
22498
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ivi#
uint32_t sl_btmesh_evt_diagnostic_friend_relay_s::ivi
IV index used to secure the message
Definition at line
22499
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
seq#
uint32_t sl_btmesh_evt_diagnostic_friend_relay_s::seq
Sequence number of the message
Definition at line
22500
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h