Data structure of the check_fw_metadata_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::elem_index
Server model element index
Definition at line
15886
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::client_address
Address of the Update Client
Definition at line
15887
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint8_t sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::fw_index
Index of the currently installed firmware to check for updating.
Definition at line
15888
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
metadata#
uint8array sl_btmesh_evt_fw_update_server_check_fw_metadata_req_s::metadata
Metadata for the incoming firmware. May be zero-length.
Definition at line
15890
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h