Data structure of the update_start_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::elem_index
Server model element index
Definition at line
15915
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::client_address
Address of the Update Client
Definition at line
15916
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_update_server_update_start_req_s::blob_id
BLOB ID of the firmware being transferred.
Definition at line
15917
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint8_t sl_btmesh_evt_fw_update_server_update_start_req_s::fw_index
Index of the firmware to update
Definition at line
15919
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
metadata#
uint8array sl_btmesh_evt_fw_update_server_update_start_req_s::metadata
Metadata for the FWID in the following update_start_req event. May be zero-length.
Definition at line
15920
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h