Data structure of the state_changed event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_generic_server_state_changed_s::elem_index
Server model element index
Definition at line
5904
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
model_id#
uint16_t sl_btmesh_evt_generic_server_state_changed_s::model_id
Server model ID
Definition at line
5905
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
remaining_ms#
uint32_t sl_btmesh_evt_generic_server_state_changed_s::remaining_ms
Time (in milliseconds) remaining before transition from current state to target state is complete. Ignored if no transition is taking place.
Definition at line
5906
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
type#
uint8_t sl_btmesh_evt_generic_server_state_changed_s::type
Model-specific state type, identifying the kind of state reported in the state change event. See get state types list for details.
Definition at line
5910
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
parameters#
uint8array sl_btmesh_evt_generic_server_state_changed_s::parameters
Message-specific parameters, serialized into a byte array
Definition at line
5913
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h