Data structure of the light_onoff_updated event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_server_light_onoff_updated_s::destination_address
Message destination address if triggered by a message, 0 otherwise.
Definition at line
14102
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_server_light_onoff_updated_s::elem_index
Index of the element where the update happened
Definition at line
14104
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
source_address#
uint16_t sl_btmesh_evt_lc_server_light_onoff_updated_s::source_address
Message source address if triggered by a message, 0 otherwise.
Definition at line
14106
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_server_light_onoff_updated_s::appkey_index
Message appkey index if triggered by a message, 0xFFFF otherwise.
Definition at line
14108
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
onoff_state#
uint8_t sl_btmesh_evt_lc_server_light_onoff_updated_s::onoff_state
The target value of the Light LC Light OnOff state.
Definition at line
14110
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
onoff_trans_time_ms#
uint32_t sl_btmesh_evt_lc_server_light_onoff_updated_s::onoff_trans_time_ms
Amount of time (in milliseconds) the element will take to transition to the target state from the present state.
Definition at line
14112
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h