Data structure of the linear_output_updated event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_lc_server_linear_output_updated_s::elem_index

Index of the element where the update happened


Definition at line 14198 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

linear_output_value#

uint16_t sl_btmesh_evt_lc_server_linear_output_updated_s::linear_output_value

The updated value of the LC Linear Output state


Definition at line 14200 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h