Data structure of the om_updated event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_server_om_updated_s::destination_address
Message destination address if triggered by a message, 0 otherwise.
Definition at line
14069
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_server_om_updated_s::elem_index
Index of the element where the update happened
Definition at line
14071
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_lc_server_om_updated_s::client_address
Message source address if triggered by a message, 0 otherwise.
Definition at line
14073
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_server_om_updated_s::appkey_index
Message appkey index if triggered by a message, 0xFFFF otherwise.
Definition at line
14075
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
om_value#
uint8_t sl_btmesh_evt_lc_server_om_updated_s::om_value
The value the LC Occupancy Mode state is being set to.
Definition at line
14077
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h