Data structure of the set_property event.

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::destination_address

Address of the server or the group address to which it was published.


Definition at line 14468 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::elem_index

Index of the element which received the command.


Definition at line 14470 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::client_address

Device which sent the request.


Definition at line 14472 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::appkey_index

Appkey used by client_address.


Definition at line 14473 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::property_id

Property ID


Definition at line 14474 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_value#

uint8array sl_btmesh_evt_lc_setup_server_set_property_s::property_value

Property value


Definition at line 14475 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h