sl_btmesh_evt_lcd_client_data#

Event reporting queried composition data page contents.

The content of the event is requested using the sl_btmesh_lcd_client_get_composition_data or sl_btmesh_lcd_client_get_metadata command. More than one event may be generated. This event preceedes by a sl_btmesh_evt_lcd_client_data_header event. Page content is terminated by a sl_btmesh_evt_lcd_client_data_end event. Note that the interpretation of the received data is page-specific.

Modules#

sl_btmesh_evt_lcd_client_data_s

Macros#

#define

Identifier of the data event.

Typedef Documentation#

sl_btmesh_evt_lcd_client_data_t#

typedef struct sl_btmesh_evt_lcd_client_data_s sl_btmesh_evt_lcd_client_data_t

Definition at line 21774 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_lcd_client_data_id#

#define sl_btmesh_evt_lcd_client_data_id
Value:
0x026600a8

Identifier of the data event.


Definition at line 21763 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h