Data structure of the capabilities event.
Public Attribute Documentation#
uuid#
uuid_128 sl_btmesh_evt_prov_capabilities_s::uuid
UUID of the device being provisioned
Definition at line
2317
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elements#
uint8_t sl_btmesh_evt_prov_capabilities_s::elements
Number of elements supported by the device
Definition at line
2318
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
algorithms#
uint16_t sl_btmesh_evt_prov_capabilities_s::algorithms
Supported algorithms and other capabilities.
Definition at line
2319
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
pkey_type#
uint8_t sl_btmesh_evt_prov_capabilities_s::pkey_type
Supported public key types
Definition at line
2320
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
static_oob_type#
uint8_t sl_btmesh_evt_prov_capabilities_s::static_oob_type
Supported static OOB Types
Definition at line
2321
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ouput_oob_size#
uint8_t sl_btmesh_evt_prov_capabilities_s::ouput_oob_size
Maximum size of Output OOB supported
Definition at line
2322
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
output_oob_action#
uint16_t sl_btmesh_evt_prov_capabilities_s::output_oob_action
Supported Output OOB Actions
Definition at line
2323
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
input_oob_size#
uint8_t sl_btmesh_evt_prov_capabilities_s::input_oob_size
Maximum size of input OOB supported
Definition at line
2324
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
intput_oob_action#
uint16_t sl_btmesh_evt_prov_capabilities_s::intput_oob_action
Supported input OOB Actions
Definition at line
2325
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h